Wrist Camera
Topic outline
-
Locate objects the fastest and easiest way with Robotiq’s Wrist Camera! The following introductory video will present you the Wrist Camera, defined by the Visiion and Vision System. The Vision System uses the Robotiq Wrist Camera and the URCap software on Universal Robots to provide you with a simple object teaching interface. The interface allows to set up the Vision System so it can recognize object locations and orientations automatically. The Camera is designed to work in industrial applications in combination with the Robotiq Hand-E, 2F-85 and 2F-140 Adaptive Grippers. Get a glimpse of what the Wrist Camera can do to help you automate your robotic tasks faster!
-
-
Optimize the object detection by creating a robust model with the advanced features of the Wrist Camera. With the built-in options, you can adjust the Camera's parameters to fit your application. Manually adjust the LED intensity, exposure, gain and white balance. Lock the focus to optimize the acquisition speed and save time in your process.
Feature Highlights
- Learn how to access the advanced Camera parameters
- Adjust the LED intensity
- Adjust the exposure and gain
- Set and lock the manual focus.
- Adjust the white balance for better validation.
How to Use the Advanced Parameters
-