Once your manual task map is done, you are ready to prepare its robotic equivalent: the robotic task map. The thing about robotic task mapping is that you can’t do it without knowing the layout and you can’t complete the layout without having the task map on hand! That’s why we recommend working on these two components together. 

The Robotic Task Mapping Template has the same structure as the manual map. Complete it and you will be ready to perform the manual-robotic comparison.

 Click here to download it!

Refer to the next lesson for information about the robotic cell layout.

Last modified: Tuesday, 28 January 2020, 2:54 PM